Add an agent computer

Use agents to perform scheduled operations. The agents can be installed on the computer running the FactoryTalk AssetCentre server, on computers running the FactoryTalk AssetCentre client, or on any other computer that meets the requirements and is connected to the FactoryTalk AssetCentre server.
To add an agent computer to the FactoryTalk AssetCentre system, simply install the FactoryTalk AssetCentre agent software on it. When you install the agent software, it is registered with the FactoryTalk AssetCentre server and can immediately run scheduled tasks. No further configuration is necessary.
To add an agent computer
  1. Use the FactoryTalk AssetCentre disc to run the installation program. If it does not start automatically, run
    Setup.exe
    from the disc.
  2. On the setup menu click
    Install FactoryTalk AssetCentre Agents
    .
  3. Follow the on screen instructions to complete the installation. For detailed instructions select
    Help > Installation Guide
    to see the
    FactoryTalk AssetCentre Installation Guide
    .
During the installation, FactoryTalk Services Platform will be installed and the computer will be added to the FactoryTalk Network Directory. If for some reason the agent computer is not in the FactoryTalk Network Directory, use the FactoryTalk Administration Console to add it. See the
FactoryTalk Administration Console Help
for instructions on adding a computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal