Log on FactoryTalk AssetCentre services with different types of accounts
When logging on the services of FactoryTalk AssetCentre server, FactoryTalk AssetCentre Agent Controller, FactoryTalk AssetCentre Inventory Crawler, and FactoryTalk AssetCentre Verification Agent as the following table, you can refer the scenarios in the table to run Disaster Recovery schedule, perform Change Detect, and execute searches.
System Architecture | FactoryTalk AssetCentre services | Account | Disaster Recovery Schedule | Change Detect | Searches |
|---|---|---|---|---|---|
Same server for FactoryTalk AssetCentre and Microsoft SQL Server | Server | NT SERVICE\FTACServer | All device types are supported. | Change Detect for Allen-Bradley Logix 5000 controller is supported. | All search types are supported. |
Agent Controller | Network Service | ||||
Inventory Crawler | Network Service | ||||
Verification Agent | Network Service | ||||
Separate servers for FactoryTalk AssetCentre and Microsoft SQL Server | Server | Standalone Microsoft Managed Service Account (sMSA), Group Managed Service Account (gMSA) | Most device types are supported. The exceptions include:
| Change Detect for Allen-Bradley Logix 5000 controller is supported. | All search types are supported. |
Agent Controller | Network Service | ||||
Inventory Crawler | Network Service | ||||
Verification Agent | Network Service |
Provide Feedback