Start an agent controller as a service
You can start an agent controller as a service using FactoryTalk AssetCentre Agent Controller Launch Control Panel.
TIP:
You can run only one agent controller service on the same agent computer at a time.
To start an agent controller as a service
- Open FactoryTalk AssetCentre Agent Controller Launch Control Panel.FromWindows Startmenu, selectRockwell Software>FactoryTalk AssetCentre Agent Controller Launch Control Panel.OrNavigate toC:\Program Files (x86)\Rockwell Software\AssetCentre Agents\AgentController, and double-clickRA.FTAC.AgentControllerLaunchPanel.exe.If displayed, clickYeswhen theUser Account Controldialog box prompts for Windows users.
- In theAgent Controller Launch Control Panelwindow, select theA Serviceoption.
- Click theSave and Startbutton.
The agent controller starts to run as a service, and all agent tasks assigned to the agent controller will start. The agent controller service starts automatically after restarting the agent computer.
Provide Feedback