Stop an agent controller's running mode
You can stop an agent controller's running mode using FactoryTalk AssetCentre Agent Controller Launch Control Panel.
To stop an agent controller's running mode
- Open the FactoryTalk AssetCentre Agent Controller Launch Control Panel.FromWindows Startmenu, selectRockwell Software>FactoryTalk AssetCentre Agent Controller Launch Control Panel.OrNavigate toC:\Program Files (x86)\Rockwell Software\AssetCentre Agents\AgentController, and double-clickRA.FTAC.AgentControllerLaunchPanel.exe.If displayed, clickYeswhen theUser Account Controldialog box prompts for Windows users.
- In theAgent Controller Launch Control Panelwindow, click theStopbutton.
The agent controller stops, and all agent tasks assigned to the agent controller will stop.
If the agent controller you want to stop is running as an application, you can also stop it from Windows notification area.
Provide Feedback