About the agent controller application icon in Windows notification area
If an agent controller is running as an application, you can find the agent controller application icon in Windows notification area. Use this icon to open FactoryTalk AssetCentre Agent Controller Launch Control Panel, or to stop the agent controller.
- Right-click the agent controller application icon in Windows notification area to show the menu items:
- Launch Control PanelSelect to show theAgent Controller Launch Control Panelwindow.
- Shut Down AssetCentre Agent ControllerSelect to exit the agent controller application, and the agent controller will stop.
Provide Feedback