Stop an agent controller's application running mode from Windows notification area

If an agent controller is running as an application, you can stop it from Windows notification area.
To stop an agent controller's application running mode from Windows notification area
  1. Right-click the agent controller application icon in Windows notification area.
  2. Select
    Shut Down AssetCentre Agent Controller
    .
The agent controller stops, and all agent tasks assigned to the agent controller will stop.
The message in the
Status text box
of the
Agent Controller Launch Control Panel
window will also be updated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal