Start an agent controller as an application
You can start an agent controller as an application using FactoryTalk AssetCentre Agent Controller Launch Control Panel.
TIP:
You can run only one agent controller application on the same agent computer at a time.
If you want to start an agent controller as an application, make sure that the agent controller application is allowed to communicate through the Windows firewall by adding
RA.FTAC.AgentControllerApplication.exe
as one of the allowed programs.To start an agent controller as an application
- Open FactoryTalk AssetCentre Agent Controller Launch Control Panel.FromWindows Startmenu, selectRockwell Software>FactoryTalk AssetCentre Agent Controller Launch Control Panel.OrNavigate toC:\Program Files (x86)\Rockwell Software\AssetCentre Agents\AgentController, and double-clickRA.FTAC.AgentControllerLaunchPanel.exe.If displayed, clickYeswhen theUser Account Controldialog box prompts for Windows users.
- In theAgent Controller Launch Control Panelwindow, select theAn Applicationoption, and then specify a Windows user account with standard user permission to run the agent controller.
- Account name input fieldEnter a Windows user account with standard user permission to run the agent controller.
- Browse buttonSelect to browse and add a Windows user account with standard user permission to run the agent controller.
- Click theSavebutton.TIP:By clicking theSavebutton, the settings you configured in theAn Applicationoption andAccount nameare saved.
The agent controller runs as an application, and all agent tasks assigned to the agent controller will start. The agent controller application will start after the next time the user logs on.
TIP:
You can also start the agent controller application by navigating to
C:\Program Files (x86)\Rockwell Software\AssetCentre Agents\AgentController
, and then double-clicking RA.FTAC.AgentControllerApplication.exe
.Provide Feedback