Add an Agent Computer dialog box

How do I open the Add an Agent Computer dialog box?
  1. If you are not in it, enter Design mode.
  2. On the
    Menu bar
    , select
    View > Agent Groups
    , or click the
    Agent Groups
    button.
  3. Select an agent group (or an agent computer under the group) where you want to add the agent computer to.
  4. Click the
    Add Agent Computer
    button on the
    Agent Group Creation and Agent Assignment
    toolbar.
    TIP:
    You can also right-click the agent group and select
    Add Agent Computer
    .
Use the
Add an Agent Computer
dialog box to create an agent computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal