Items in Add an Agent Computer dialog box
Items in the dialog box include:
- NameThe name for the agent computer. It is not editable after creation and must be unique under the same agent group.
- LocationThe location for the agent computer.
- Description(optional) The description for the agent computer.
- Test Connection(optional) Click theConnectbutton to check whether the FactoryTalk AssetCentre Server service can connect to the agent computer.
Provide Feedback