Agent Computer Properties dialog box
How do I open the Agent Computer Properties dialog box?
- If you are not in it, enter Design mode.
- On theMenu bar, clickView > Agent Groups(or click theAgent Groupsbutton).
- In theAgent Group Creation and Agent Assignmentpane, select the agent computer you want to edit.
- Click thePropertiesbutton on theAgent Group Creation and Agent Assignmenttoolbar.TIP:You can also right-click the agent computer you want to edit and selectProperties.
Use the
Agent Computer Properties
dialog box to change the properties of an agent computer. (If you are not in Design mode, and you have Read
permission, you will be able to view but not edit the properties.)Provide Feedback