Items in Agent Computer Properties dialog box

Items in the dialog box include:
  • Name
    The name of the agent computer. It is not editable after creation and must be unique under the same agent group.
  • Location
    The location for the agent computer.
  • Description
    (optional) The description for the agent computer.
  • Test Connection
    (optional) Click
    Connect
    button to check whether the FactoryTalk AssetCentre Server service can connect to the agent computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal