Move an asset
You can move an asset from one agent group into another.
To move an asset
- If you are not in it, enter Design mode.
- On theMenubar, clickView > Agent Groups(or click theAgent Groupsbutton).
- In theAsset per Agent Grouppane, select an asset you want to move. To select multiple assets, useCtrl-ClickorShift-Click.TIP:You can also select an agent group under which all the assets you would like to move to other agent group. To select multiple agent groups, useCtrl-ClickorShift-Click.
- Right-click the selection and select the agent group you want to move the assets to.
- When prompted to move the assets, confirm the list of assets to be moved, and clickOK.TIP:If the asset you move inherits the agent group from its parent, its Agent Group property will be changed fromInherit from parentto the target agent group. If the asset you move is a parent and has child assets inherit agent group from it, the child assets will move together with the parent to the target agent group.
Provide Feedback