Graphics Editor

Use the Graphics editor to create or edit displays.
The Graphics editor provides a drawing area that represents the displays, and a variety of graphic tools that are available from the menus, toolbars, and palettes in the Graphics window.
You can create standard graphic displays (in the
Displays
folder), global object displays (in the
Global Objects
folder), and library displays (in the
Libraries
folder).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal