Set up a graphic display
You can set up options to specify the appearance of a display at runtime.
To set up a graphic display:
- On the display, selectEdit>Display Settings.
- In the Display Settings dialog box, set up options to define settings like size and background color. Some display settings also determine how the screen will look and behave at runtime.
- On the display, selectViewand select commands such as Zoom in or Zoom out to increase or reduce the magnification of the graphic display. Magnification is not retained between editing sessions.TIP:When you change the size or location of a display and save it, the information in Display Settings is changed to reflect this.If you select an existing display when you start the editor, the display determines the size and location of the editor's window. Otherwise these are determined by the most recently edited graphic display. You can have multiple graphic displays open at one time.
Provide Feedback