Set up the Graphics window
You can set up the Graphics window to show or hide the toolboxes, toolbars, and palettes. You can also set up and activate a grid that you can use to assist in the placement of objects on a display.
TIP:
The settings apply to the Graphics window rather than the individual displays and stay as you set them from one editing session to the next.
To set up the Graphics window:
- In the Graphics editor, selectView.
- On the menu items, select or clear items that you want to set up.
Provide Feedback