Magnify a display
The
Zoom In
option on the View
menu allows you to magnify one or more objects in a graphic display in more detail, making it easier to draw.
TIP:
Use the
Cancel Zoom
option to return the display to its original size.To magnify objects:
- InFactoryTalk View Studio, in theGraphicseditor, select the object or objects to magnify.
- SelectView>Zoom In. The selected objects will be centered in the magnified view of the display.
- Use the scroll bars to view areas of the graphic display that are not immediately visible.
To magnify the display:
- InFactoryTalk View Studio, in theGraphicseditor, right-click anywhere in the display and selectDisplay Settings.
- In theDisplay Settingsdialog box, in thePropertiestab, make sure theSizeproperty is set toSpecify Size in Pixels.
- In theGraphicseditor, in the editing window, drag the sides of the display to enlarge it to the required size. Dotted lines indicate the display's original size.
- Right-click the display and clickZoom to Fit. The display is resized maintaining its aspect ratio, or relative sizes and positions of the objects in the display.TIP:If theSizeproperty is set toUse Current Size,Zoom to Fitbehaves the same as Cancel Zoom.
Provide Feedback