Specify the display settings

In the
Display Settings
dialog box, you can set up how the current graphic display look and behave at runtime
To specify the display settings:
  1. In the
    Properties
    tab, specify the details of how the display will look at runtime.
  2. In the
    Behavior
    tab, specify how the display will behave at runtime.
  3. Click
    OK
    to save the settings and close the dialog box when setup is complete.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal