Change the default display settings

In the
Display Settings
dialog box, you can specify that the settings for the current graphic be used as default display settings.
To change the default display settings:
  1. In the
    Properties
    or
    Behavior
    tab, specify changes to the settings to whatever you intend the default settings to be.
  2. Click
    Set as Default
    to make the current display settings the default for new displays.
    TIP:
    When you make a background color change to display settings, the
    Set as Default
    button changes to
    Apply
    . You can use this to apply the change you made without closing the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal