Edit display runtime behavior

Use the
Behavior
tab to edit the settings.
To edit runtime behavior settings for a display:
  1. In the
    Display Settings
    dialog box, click the
    Behavior
    tab.
  2. Edit the settings presented in this tab:
    • Startup and shutdown commands
    • Colors for input fields
    • The behavior of interactive objects, such as push buttons
    • The behavior of objects with input focus
    • The availability of an on-screen keyboard
    • The availability of button action when an error has been raised
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal