Open Symbol Factory
Symbol Factory provides a large number of graphic objects to be used in graphic displays.
To open Symbol Factory, do one of the following:
- In the Explorer window, expand the HMI server. Under theGraphicsfolder, double-clickSymbol Factory.
- From the menu, selectObjects>Symbol Factory.
- In the Toolbox, click the Symbol Factory icon
.
Provide Feedback