Use objects from Symbol Factory

Symbol Factory provides a large number of graphic objects that you can use in your graphic displays.
To use objects from Symbol Factory:
  1. Open the graphic display you intend to put the object on.
  2. Open Symbol Factory.
  3. In the
    Categories
    pane, select a category of graphics.
  4. Select a graphic by clicking its thumbnail.
  5. (optional) For enhanced symbols, edit the color or parts of the graphic.
  6. Click on the Copy options from the context menu for the desired format.
  7. Paste the graphic to your graphic display or an Image object on the display.
    You can drag basic symbols from Symbol Factory to your graphic display directly.
    You can also export symbols to a variety of file formats.
For more information, click
Help
in the Symbol Factory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal