About Symbol Factory

Symbol Factory is a library of over 5,000 graphics for industrial automation, including pumps, pipes, valves, tanks, mixers, motors, ducts, electrical symbols, flow meters, material handling, sensors, PLCs, transmitters, and ISA symbols.
In Symbol Factory,you can switch between two types of symbols:
  • Basic symbols
    Includes a format of Windows Metafile (WMF) or bitmap image file (BMP).
  • Enhanced symbols
    Includes a format of scalable vector graphics (SVG) and contains gradients.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal