View the entire display

You can resize a graphic display so all of its objects fit into the current window.
To view the entire display:
  1. In the
    Graphics
    editor, click the display to make it active.
  2. Select
    View
    >
    Zoom to Fit
    .
    TIP:
    This view might distort the aspect ratio of the objects. Editing with this view is not recommended.
    Use
    Cancel Zoom
    to return the display to its starting size.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal