Change graphic library location
By default, the library files are stored in
C:\Users\Public\Documents\RSView Enterprise\SE\Libraries
. After you change the folder location, any new library displays you create will be saved to the new location. The original contents of the library will have to be moved to the new location using Windows Explorer, or added to the new library folder using Add Component into Project
, just as you would add any other graphic display.To change the folder location of graphic library files:
- In FactoryTalk View Studio, clickTools>Options.
- In theOptionsdialog box, click theBrowsebutton.
- In theBrowse For Folderdialog box, specify the new location and clickOK.
Provide Feedback