FactoryTalk alarm and event monitoring
With
FactoryTalk Alarms and Events
, a FactoryTalk View
application can include the following alarm monitoring:- Device-based alarms, including:
- Logix instruction-based alarmsAlarm instructions are programmed and then downloaded into theStudio 5000controllers. The controller detects alarm conditions and publishes the alarm information, which is routed toFactoryTalk Alarms and Events.
- Logix tag-based alarmsLogix tag-based alarms associate alarm conditions with tags forStudio 5000controllers. Logix tag-based alarms monitor tag values to determine the alarm condition, but they are not part of the logic program and do not increase the scan time for a project. Logix tag-based alarms are supported only onCompact GuardLogix5380,CompactLogix5380,CompactLogix5480,ControlLogix5580, andGuardLogix5580 controllers.
- Server tag-based alarmsAlarm conditions are defined and managed with software that monitors programmable controllers through tags. Tag-based alarm monitoring is supported byRockwell Automationcontrollers communicating throughRockwell Automationdevice servers (FactoryTalk Linx), third-party controllers communicating through OPC data servers, and HMI tags. Use server tag-based alarm monitoring if you do not want to use the pre-built instructions in Studio 5000 Logix Designer, or do not have Studio 5000 controllers.
- OPC UA alarmsAlarm conditions are provided by third-party OPC UA servers. The alarm data is then routed toFactoryTalk Alarms and Eventsthrough FactoryTalk Linx OPC UA Connector.
For more information about FactoryTalk alarm and event monitoring, see
FactoryTalk Alarms and Events Help
.Provide Feedback