Turn on multiple languages in graphic library
If you turn on multiple language support for a graphic library, when you save the graphic library display, all strings that support language switching are saved in the application's current language. If you turn off the support, only text strings using the current application language will be saved.
To turn on multiple language support in graphic libraries:
- In Factorytalk View Studio, under the HMI server, expandGraphics>Librariesand double-click the library component that is to support multiple languages.
- On the library display, right-click and selectDisplay Settings.
- In theDisplay Settingsdialog box, on thePropertiestab, select theSupport Multiple Languagescheck box.
- ClickOK.
Provide Feedback