Create a library component

You can create a library component in the Graphics Libraries so that you can use it easily in your graphic displays.
To create a library component:
  1. In FactoryTalk View Studio, under the HMI server, expand
    Graphics
    , right-click
    Libraries
    and select
    New
    .
  2. In the graphics editor, create or edit the display.
  3. When complete, save the display.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal