Add an existing graphic library

You can add an existing graphic library (*.gfx or *.ggfx) to the Graphic Libraries.
To add an existing graphic library:
  1. In FactoryTalk View Studio, under the HMI server, expand
    Graphics
    , right-click
    Libraries
    and select
    Add Component into Project
    .
  2. In the
    Add Component into Project
    dialog box, navigate to the graphic you want to add and then click
    Open
    to copy the library into the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal