New Condition dialog
How do I open the Conditions tab?
- OnSearches, select the search to contain the new condition.
- SelectDetailed settings > Conditions.
- SelectNew condition.
Use the
New Condition
dialog to create a search condition. You can use the
Column
field to select the data property for which you are creating the
condition, and then complete the dialog options for the selected data property. The
following table shows the data sources and their columns.Data Sources | Columns |
|---|---|
Archive Check In & Check Out Status | |
Asset Extended Property | |
Provide Feedback