Condition - Occurred Time dialog
How do I open the New Condition - Occurred Time dialog?
- OnSearches, select the search, whose data source isAudits,Diagnostics and Health, orEvents.
- SelectDetailed settings > Conditions.
- SelectNew condition.
- SelectOccurred Timefrom theColumnlist.
Use the
New Condition - Occurred Time
dialog to create or modify a condition that
searches for log records with a specific occurred Time. For example, within the last
three days, after three days ago, or between specific dates such as April 7 and 14,
2007.Provide Feedback