Condition - File Name dialog
How do I open the New Condition - File Name dialog?
- OnSearches, select the search, whose data source isArchive Check In & Check Out Status.
- SelectDetailed settings > Conditions.
- SelectNew condition.
- SelectFile Namefrom theColumnlist.
Use the
New Condition - File Name
dialog to create or modify a condition that
searches for log records generated with a specific file name.Provide Feedback