Condition - Computer\Location dialog
How do I open the New Condition - Computer\Location dialog?
- OnSearches, select the search, whose data source isArchive Check In & Check Out Status.
- SelectDetailed settings > Conditions.
- SelectNew condition.
- SelectComputer\Locationfrom theColumnlist.
Use the
New Condition - Computer\Location
dialog to create or modify a condition
that searches log records for the computer or location from which a file was checked
out.Provide Feedback