Condition - Message dialog

How do I open the New Condition - Message dialog?
  1. On
    Searches
    , select the search, whose data source is
    Audits
    ,
    Diagnostics and Health
    ,
    Events
    .
  2. Select
    Detailed settings > Conditions
    .
  3. Select
    New condition
    .
  4. Select
    Attachments
    from the
    Column
    list.
Use the
New Condition - Message
dialog to create or modify a condition that searches for log records with specific message text, for example, the word create could determine when an asset or file was added to the asset tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal