Condition - Logged Time dialog
How do I open the New Condition - Logged Time dialog?
- OnSearches, select the search, whose data source isAudits,Diagnostics and Health, orEvents.
- SelectDetailed settings > Conditions.
- SelectNew condition.
- SelectLogged Timefrom theColumnlist.
Use the
New Condition - Logged Time
dialog to create or modify a condition that
searches for log records with a specific logged time (the date the FactoryTalk
AssetCentre database received report of the event from the software product; for
example, in the last three days or between specific dates like April 7 and 14,
2007).The logged time and occurred time may be different if you disconnect from the network
while FactoryTalk AssetCentre caches data, or if the time on the server is different
than the time on your computer.
Provide Feedback