Condition - Resource dialog
How do I open the New Condition - Resource dialog?
- OnSearches, select the search, whose data source isAuditsorDiagnostics and Health.
- SelectDetailed settings > Conditions.
- SelectNew condition.
- SelectResourcefrom theColumnlist.
Use the
New Condition - Resource
dialog to create or modify a condition that
searches for log records generated by a specific resource (software product).
TIP:
Resource is the name of the hardware or software object to which the action happened,
such as the name of the processor that went online or the name of the file that was
saved. Therefore, resource and source have the potential of being the same software
product that logs an entry.
Provide Feedback