Condition - User Name dialog
How do I open the New Condition - User Name dialog?
- OnSearches, select the search, whose data source isArchive Check In & Check Out Status,Archive History,Audits, orDiagnostics and Health.
- SelectDetailed settings > Conditions.
- SelectNew condition.
- SelectUser Namefrom theColumnlist.
Use the
New Condition - User Name
dialog to create or modify a condition that
searches for log records generated when a specific user name was logged on to the
computer that generated the Audit Log record.Provide Feedback