Condition - Source dialog

How do I open the New Condition - Source dialog?
  1. On
    Searches
    , select the search, whose data source is
    Audits
    ,
    Diagnostics and Health
    , or
    Events
    .
  2. Select
    Detailed settings > Conditions
    .
  3. Select
    New condition
    .
  4. Select
    Source
    from the
    Column
    list.
Use the
New Condition - Source
dialog to create or modify a condition that searches for log records generated by a specific source, such as the software product Logix Designer.
TIP:
Resource, while sometimes the name of the hardware object to which the action happened, can also be a software product. Therefore, the source and resource can be the same software product that logs an entry.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal