Condition - Location dialog

How do I open the New Condition - Location dialog?
  1. On
    Searches
    , select the search, whose data source is
    Audits
    ,
    Diagnostics and Health
    , or
    Events
    .
  2. Select
    Detailed settings > Conditions
    .
  3. Select
    New condition
    .
  4. Select
    Location
    from the
    Column
    list.
Use the
New Condition - Location
dialog to create or modify a condition that searches for log records with a specific location from which records were reported, for example, a computer named Workstation1.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal