Search
FactoryTalk View SE Help
Animating graphic objects
To animate FactoryTalk View objects in a graphic display, create the objects first, and then apply animation to them.
Adding Animation to Graphic Displays
Setting up color animation
Color tab
Options on the Color tab
Options of Fill Style
Set up fill animation
Options in the Fill tab
Set up height animation
Options in the Height tab
Set up width animation
Width tab
Options on the Width tab
Set up horizontal motion for an object
Options on the Horizontal Position tab
Set up vertical motion for an object
Vertical Position tab
Options on the Vertical Position tab
Set up hyperlink animation
Options on the Hyperlink tab
Configure IIS for hyperlink animation
Example: Address of hyperlinks
Set up rotation for an object
Options in the Rotation tab
Set up visibility animation
Visibility tab
Set up touch animation for an object
Touch tab
Options in the Touch tab
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal