Set up width animation
Use the
Width
tab to set up the width animation for an object.If a group object and the objects within a group object have width animation set up, animation results for the individual objects and the group are combined. Be sure to test group animation to ensure that it produces the effect you intend.
To set up width animation:
- In theWidthtab, in theExpressionfield, type a tag name or an expression that will return numeric values at runtime. You can also clickTagto browse for a tag, or clickExpressionto open theExpression Editorto create one.
- Specify the fields ofExpression Range,Horizontal change (Percent), andAnchor, as described in the options below.TIP:You can also use the Object Smart Path feature to set these values.
Provide Feedback