Options on the Width tab
The following table shows options on the tab.
Options | Description |
---|---|
Expression | Specify a tag name or an expression that will evaluate to numeric values at runtime. An expression is a mathematical or logical equation that returns a value. It can contain tag names; constants; mathematical, relational, logical and bitwise operators; and built-in alarms and events functions. A tag name can be used as an expression. |
Expression range | Specify the range of values for the expression, including:
|
Horizontal change (Percent) | Specify the minimum and maximum percentage of horizontal change.
|
Anchor | Specify which part of the object remains constant, including:
|
Provide Feedback