Visibility tab

How do I open the Visibility tab
In
FactoryTalk View Studio
, in the
Graphics
editor, right-click the object and then select
Animation
>
Visibility
.
Use the
Visibility
tab to specify that an object become visible or invisible as a tag value, or the result of a logical expression, changes.
The following table shows options on the tab.
Options
Description
Expression
Specify a tag name or an expression that will evaluate to
True
(any non-zero value) or
False
(zero) at runtime.
An expression is a mathematical or logical equation that returns a value. It can contain tag names; constants; mathematical, relational, logical and bitwise operators; and alarm functions.
A tag name can be used as an expression.
Expression true state
Specify whether the object is to be visible or invisible when the expression returns
True
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal