Set up horizontal motion for an object

Use the Horizontal Position option on the Animation menu to move an object horizontally as a tag value or the results of an expression change. The horizontal position of the object is proportional to the value of the expression. For example, if the value of the expression is halfway between its minimum and maximum values, the horizontal position of the object will be halfway between its minimum and maximum horizontal offset positions.
TIP:
If a group object and the objects within a group object have horizontal animation set up, animation results for the individual objects and the group are combined. Be sure to test group animation to ensure that it produces the effect you intend.
To set up horizontal motion for an object:
  1. In the
    Graphics
    editor, right-click the object and then click
    Animation
    >
    Horizontal Position
    .
  2. In the
    Animation
    dialog box, in the
    Horizontal Position
    tab, in the
    Expression
    field, type a tag name or an expression that will return numeric values at runtime.
    You can also click
    Tag
    to browse for a tag, or click
    Expression
    to open the
    ExpressionEditor
    to create one.
  3. Specify
    Expression Range
    , and
    Horizontal offset (Pixels)
    , as described in the options below. You can also use the Object Smart Path feature to set these values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal