Width tab

How do I open the Width tab
In
FactoryTalk View Studio
, in the
Graphics
editor, right-click the object and then select
Animation
>
Width
.
Use the
Width
option on the
Animation
menu to change the width of an object as a tag value or the result of a logical expression changes. The width of the object is proportional to the value of the expression. For example, if the value of the expression is halfway between its minimum and maximum values, the width of the object will be halfway between its minimum and maximum horizontal change percents.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal