Vertical Position tab

How do I open the Vertical Position tab
In
FactoryTalk View Studio
, in the
Graphics
editor, right-click the object and then select
Animation
>
Vertical Position
.
Use the
Vertical Position
option on the
Animation
menu to move an object vertically as a tag value or the results of an expression change. The vertical position of the object is proportional to the value of the expression. For example, if the value of the expression is halfway between its minimum and maximum values, the vertical position of the object will be halfway between its minimum and maximum vertical offset positions.
If a group object and the objects within a group object have vertical animation set up, animation results for the individual objects and the group are combined. Be sure to test group animation to ensure that it produces the effect you intend.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal