Set up vertical motion for an object

Use the
Vertical Position
tab to set up how to move an object vertically as a tag value or the results of an expression change.
To set up vertical motion for an object:
  1. In the
    Vertical Position
    tab, in the
    Expression
    field, type a tag name or an expression that will return numeric values at runtime. You can also click
    Tag
    to browse for a tag, or click
    Expression
    to open the
    Expression Editor
    to create one.
  2. Specify
    Expression Range
    and
    Vertical offset (Pixels)
    . You can also use the Object Smart Path feature to set these values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal