Use the Alarm and Event Summary at runtime
During runtime an operator can use the Alarm and Event Summary to acknowledge, disable, suppress, shelve, unshelve, filter, and sort alarms.
During design time the Alarm and Event Summary can be configured to only contain selected toolbar buttons which limits the operations available during runtime. If a toolbar button is not included in the display, the equivalent operation is also not available on the context (shortcut) menu.
Use the following keyboard shortcuts to operate the Alarm and Event Summary without a mouse at runtime.
Use this key | To do this |
---|---|
Home | Select the first item in the event list. |
End | Select the last item in the event list. |
Up Arrow | Select the previous alarm in the event list. |
Down Arrow | Select the next alarm in the event list. |
Provide Feedback