View alarm details (Summary)

At runtime, operators can view alarm details for a specific alarm in the event list portion of the Alarm and Event Summary. The
Alarm Details
dialog box shows information about all alarm conditions for the selected alarm, including the last comment that was entered for an operation.
To view alarm details for a specific alarm in the event list
  1. In the event list, select the alarm you want to view.
  2. On the toolbar, click the
    Alarm details
    BUTTON_Show_alarm_details button or right-click an alarm and then click
    View Alarm Details
    .
  3. Click
    OK
    to close the
    Alarm Details
    dialog box.
    TIP:
    The Alarm and Event Summary can be configured to hide the
    Alarm details
    toolbar button, which also hides the equivalent operation on the context (shortcut) menu.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal