Enable alarms
Enabling an alarm notifies the operator when the alarm condition occurs.
The ability to enable an alarm is controlled by
FactoryTalk Security
.To enable alarms in an application or area, you need the following security permissions for the application or area:
- Common > Read(required to list the alarm in the application or area)
- Common >List Children(required to list the alarm in the application or area)
- Alarming > Enable/Disable
To enable alarms
- On the toolbar, click theDisplay the Alarm Status Explorer
button or right-click an alarm and click
Alarm Statusto open the Alarm Status Explorer. - From theAlarm Status Explorerwindow, select the alarm or alarms you want to enable, and then click theEnable selected alarm
button.
Provide Feedback