Manage applications

Use
FactoryTalk Administration Console
to add, edit, and delete applications. Applications can be either network or local.
  • Log on to a
    FactoryTalk
    network directory to create network applications.
  • Log on to a
    FactoryTalk
    local directory to create local applications.
Once an application is created, configure it by:
  • Adding areas to the application to organize the components of the application.
  • Adding a server to an application or an area to create a link between the server and the
    FactoryTalk Directory
    .
  • Adding a logical name when the permissions associated with the logical name are inherited from that application.
  • Deleting a server or a logical name when the application no longer requires them.
    IMPORTANT:
    Managing applications requires explicit permissions. To verify permissions, in
    FactoryTalk Administration Console
    Explorer
    , right-click the
    FactoryTalk Directory
    , either network or local, and then select
    Security.
    Confirm the permissions listed in the prerequisites for the task are present with the logged in user account.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal